This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM51772: spec check

Part Number: LM51772


Tool/software:

Hi 

What is the DRV function of LM51772? Will not using it affect the OCP function?

Thanks

  • Hi Gareth,

    The DRV signal is just an optional pin/signal which can be used for an disconnect FET. If not needed just leave this open.

    This is completely separate to the OCP function.

    Best regards,

     Stefan

  • Hi Stefan

    Could you help the check below LM51772 schematic and any need to adjust

    LM51772 Buck-Boost Quickstart Tool V1_1_1_20W.xlsmLM51772 Buck-Boost Quickstart Tool V1_1_1_65W.xlsm

  • Hi Gareth,

    Please see below my review list and bold marked line items which should be checked again 

    • Checked with Quickstart Calculator

    • Rcs in series with inductor and before inductor
    • Check filter for Rcs
      Current sense Resistor Rcs does not have the required filter
    • Check filter for Risns
      Current sense Resistor Risns does not have the filter - recommend to add place holder
    • Connect IMONOUT to VCC if ISNS not used
    • Snubber on SW1 and SW2
      Place Footprint for a snubber at SW1 and SW2
       (they can then be populated in case needed (e.g. due to EMI) without layout change)
      Note: Snubber connect Resistor to GND for better Thermal performance
    • BIAS connected
      If BIAS is not used connect to GND or VIN of VOUT (do not keep open)
    • Add Series Resistor into MOSFET Gate signals lines
      (they can then be replaced in case needed (e.g. due to EMI) without layout change,
      additional option: add a diode in parallel for slow on and fast off.
    • Voltage rating of MOSFET
      (Have a margin of 30% is recommended)
    • Miller Plateau of MOSFETs
      used MOSFETs need to be logic level MOSFETs - can be seen by Miller Plateau in the range of 2.5V-3.5V
    • UVLO setting relative to lowest input voltage
      UVLO is set to xV but operating range starts at xV - relative large distance
    • Cap at VCC 22uF : (Datasheet min: 6uF with DC Bias)
      please check the cap on Vcc to have the required capacitance considering DC BIAS - we use a 22uF on the EVM
    • VCC2 is for control and driver supply
      VCC1 can used for external logic - if not used can be disabled
    • Feedback divider identical for FB and FBIN (check if FBIN is required)
    • FB_IN required: for pass through mode - only with external FB divider. With internal FB (FB connected to VCC2) put this to AGND
    • LM51772: Connect FB to VCC2 if voltage should be set via I2C  -> please check if VOUT should be set via I2C
    • nRST if not used needs to be connected to VIN

     

    65W design:

    Phase margin is low for 6V input.

    Better with 

    20W design:

    Phase margin is low for 6V input.

    Better with 

    Notes:

    - it is not clear what should assembled and what not - e.g. check components on FB

    - Device is LM51772RHAR (not PLM51772RHAR)
    - could not track signals as search did not work in pdf of schematic

    - adding a resistor divider on EN_UVLO between VIN and GND would allow to disable the LM51772 when input is low. To disable via Controller pull pin low via a Diode. Note: might need to be protected with a Zener for high input voltages.

    - a newer version of the quickstart calculator has been published

    For layout guidelines the layout please have a look at this application report first: https://www.ti.com/lit/pdf/slvafj3

    Best regards,

     Stefan

  • Hi Stefan

    Thank you for your comments,

    we will make adjustments In addition, EVM is currently used to use i2c address 0xA to adjust OCP, but the actual measurement seems to be very different. Any suggestions?

  • Hi Gareth,

    sorry, I did not understood the question about the OCP. Can you add more details?

    Best regards,

     Stefan

  • Hi Stefan

    We currently control the current limit through i2c (Address = 0xA) and find that the current cannot be set.

    Do you have any suggestions on which register to set?

  • Hi Gareth,

    the current limit can be set via I2C with this registers:

    8.2 ILIM_THRESHOLD Register (Address = 0xA) [Reset = 0x64

    But you also need to enable :

    IMON_LIMITER_EN - should be set per default

    and disable:

    SEL_ISET_PIN  in MFR_SPECIFIC_D9

    Note: please ensure you have the right filter connected to ILIM for control of current limit via DAC

    Best regards,

     Stefan