Part Number: AFE7225
Tool/software:
I was looking through SLOA229 ("Working with DC coupled Clock pins in AFE7225") and saw that it was mentioned that the VCM buffer on the chip may not come up if the input signal is not large enough in amplitude to allow for proper clock detect. This application note seems to focus on single-ended clock input, but this old thread seems to imply there are also problems with differential inputs.
In my design I am planning to drive the clock inputs with an AC-coupled LVDS signal (~ 400 mVpp single-ended) and am wondering if I must include writing to register 0xD8 bit 5 as part of the initialization sequence in order to reliably initialize the VCM buffer, or if this behavior has been fixed since that original thread was created?