This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Dear Mr./Mrs.
I have encountered problematic behaviour with different voltage supply. Design was made with 3V0 linear regulator but ADS wont start and its function of SPI seems stucked. When i use 3V3 regulator instead, everything runs normal (ads setup measurement biases etc.)
At the power up of the whole device, reset pulse is issued and than waiting few milliseconds to request device ready state over SPI communication and it always fails. (3V0 regulator)
When 3V3 regulator used, the same sequence results in successfull device ready bit reading.
Both ADS and uC(cc2652p) are supplied from the same 3V0 or 3V3 rail. SPI mode selected according to datasheet (CPOL0 CPHA1)
Few experiments were carried out (startu up timing, reset etc.) always fail with 3V0 supply.
schematic included
Looking forward to your response. Thanks!
Hi Jan Chalupa,
Can you try removing the inductor from AVDD, replace with a 0ohm resistor or otherwise short the pads together, and try again with the different power supplies? Also, you can try with a bench supply instead of the LDOs just to make sure there is not an issue with the power supply circuit.
You should also add a pull-up to DVDD on RESET so the ADC starts in a known state
-Bryan