This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I am in the process of evaluating ADS52J90EVM with TSW14J50 data capture and HSDC Pro software. However, ADS52J90 is not listed in the HSDC Pro software. Moreover, there is no initialization file for ADS52J90EVM with TSW14J50 in the HMC-DAQ GUI. I tried by modifying config files in HSDC Pro but it was not successful. I tried using JESD config but sometimes it does not syc and when in sync the data capture is not correct.
Sharing the guidelines for evaluating ADS52J90EVM with TSW14J50 along with correct config files would appreciated.
Best regards.
Hi,
Thanks for reaching out, Initially ADS52J90EVM was working with TSW1400EVM .Since this is obsolete now we had migrated to TSW14J50 . One more additional steps need to be taken to work with TSW14J50 . Can you please drop a mail to ultrasound_rx-support@list.ti.com so that we can share the extra steps.
Hi Sachin, I have received the additional steps and docs through email. However, i am not able to get the software Setup_ADS52J91_EVM_v1.0.0.exe. Could you send me this software or the link to download this software. Is this software compatible with ADS52J90EVM? ADS52j90 and ADC52J91 are the same family, I believe both are pin compatible and same interface.
You can use Setup_ADS52J90_EVM exe only . I think you have already have this file .
I am also banging my head at this problem. Could this magic .exe be made public please?
Hi Sachin, any update on the Setup_ADS52J91_EVM_v1.0.0.exe . Could you send us the access as soon as possible.
So, its not going public? People in the future should just contact TI to obtain this magic .exe?