This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3683EVM: Is it supported by TSWDC155EVM?

Part Number: ADC3683EVM
Other Parts Discussed in Thread: TSWDC155EVM, DATACONVERTERPRO-SW, TSW1418EVM

Tool/software:

Hello,

Please, does TSWDC155EVM already support ADC3683EVM?

When connecting ADC3683EVM together with TSWDC155EVM, will the current version of application DATACONVERTERPRO-SW (https://www.ti.com/tool/DATACONVERTERPRO-SW) allow me to capture samples from the ADC? (Note that TSWDC155EVM is not mentioned on the webpage of the application, but the discussion threads linked below indicate that there might be the support already).

By using this application, how long signals (or how many samples) can be recorded considering the sampling frequency of 65 MHz, 18-bit resolution, with disabled decimation, and simultaneously capturing both channels?

Moreover, is there please any other FPGA board which can be used for an evaluation of ADC3683EVM? Do you provide an IP core for this FPGA board for interfacing with this ADC?

Please note that this question is related to the following ones:

Thank you and best regards,

Ondrej