Part Number: TSW14J57EVM
Tool/software:
Hello E2E Experts,
Good day.
I tried the steps in that forum post (in the word document shared therein), and quickly realized that it is for a different version of the board. The provided solution is for the 14J57revE but we have the 14J59revB. Looking into the firmware files, it turns out that the 14J59revB does not have the indicated folder from the directions (a "DAC" folder), and there are in fact no .ini files (which the solution suggests replacing with the provided .ini file) -- only a "Firmware" folder with .bit files. Is there any chance you could generate a .bit file that performs the same firmware alteration to make a sync signal come out of the SyncC port at the end of every bitstream repetition? Even if we perform the board alteration to DC coupling, we will need to synchronize this board with two arbitrary waveform generators which will operate in tandem. If we could input an external Sync signal, that would solve this as well.
Regards,
TI-CSC