Hi,
I am using a TSW14J57EVM+DAC3XJ8 boards. I am transmitting a repetitive 4K samples long OFDM signal into an external power amplifier doing some specific linearity tests and in order to improve the scopes signal to quantization noise I use acquisition averaging. The Signal BW is high and the scope's internal trigger mechanism is not accurate enough, so I need a trig out from the pattern generator.
And there comes the question- Is there any possibility to generate a TRIG OUT signal from the TSW14J57EVM when it is connected to a DAC EVM? I see there are trigger options when using an ADC, but they are shaded when using a DAC. (It doesn't have to be a nicely placed SMA, If it is just probing a specific point on the EVM that would be great too).
Thanks
Amir