Part Number: ADC12DJ3200
Tool/software:
Hi,
My customers are facing a problem when trying to use DJ3200 in a test mode. They tried to enter the test mode with N'=12, and the data they captured for each channel is as below figure1. The Pattern for DA0-DA3 is begin with F00/E11/D22/C33 instead of in the datasheet showed F01/E11/D21/C31. Are my customers correctly entering into the test mode? Are there anything else need to configure or any reasons that can cause the customers' scenario?
Pls give some suggestions on that, thanks.


BR,
Manu