Tool/software:
Hi, I created a circuit with the help of Some TI assistance and the resulting setup of the circuit bellow. The problem im noticing with the circuit is once the Device receives 5v it gets very hot and when the 12v is plugged in it makes a squealing sound. Ive checked on the connections everywhere and it seems like the real circuit follows the schematic So im wondering if there is anything off with the schematic or something else