This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
My customer has questions about SPI as follows.
Q1:
After how much time from power up is SPI interface ready to access?
Q2:
Should SCLK, CS and DIN pins be pulled up to VD with resisters?
Best regards,
K.Hirano
Hi Hirano-san,
1. The SPI interface is ready to access once V_D is fully ramped up. A prerequisite to this is the power-supply sequence as described in section 9.1 of the datasheet.
2. The SPI pins do not need to be pulled up to VD with resistors. They are driven push-pull by the microcontroller. It might be preferred to add a pull-up resistor to ~CS so that the device is in a known state if the controller is reset, but this is not a requirement.
Regards,
Joel