Número de pieza: DAC8812
Herramienta/software:
Hello,
I have a problem with the DAC output: it always stays at 0 volts. To provide some context, I designed and prototyped two bipolar voltage sources using the DAC8812 and two OPA2277 (based on the bipolar output circuit of the DAC8811).


LDAC#: GPIO04
CS#: GPIO05
RS#: GPIO16
CLK: GPIO18
SDI: GPIO23
MSB: connect to ground
VDD: 3,3 V of ESP32
VREFX: 2,5 V of power supply
+VS: 10 V of power supply
-VS: -10 V of power supply
Estas son las señales que veo en el osciloscopio: 
First signals:
Yellow signal: CS#
Blue signal: CLK

Second signals:
Yellow signal: LDAC# (Has a duration greater than 20 ns)
Blue signal: CS#

Third signal:
Yellow signal: CLK
Blue signal: SDI (sending 0b111111111111111111)
The SPI communication initially seems good, but I can't understand why the output is different from 0 V.
/*Demo codes for testing DAC8812*/
#include <Arduino.h>
#include <SPI.h>
//Full functionality demo code
// DAC8812 Pin Definitions
#define CS_PIN 5 // Chip Select (CS) pin
#define LDAC_PIN 4 // Load DAC (LDAC) pin
#define RS_PIN 16 // Reset (RS) pin
// SPI settings
SPISettings DAC8812_settings(1000000, MSBFIRST, SPI_MODE0);
void setup() {
// Initialize Serial Monitor for debugging
Serial.begin(115200);
// Configure SPI
SPI.begin(); // Initializes the SPI bus
// Configure control pins
pinMode(CS_PIN, OUTPUT);
pinMode(LDAC_PIN, OUTPUT);
pinMode(RS_PIN, OUTPUT);
// Set control pins to default states
digitalWrite(CS_PIN, HIGH); // CS should be high when not communicating
digitalWrite(LDAC_PIN, HIGH); // LDAC high to not update outputs
digitalWrite(RS_PIN, HIGH); // RS high to avoid reset
Serial.println("DAC channels updated!");
}
void loop() {
// Your main loop code can go here
//digitalWrite(RS_PIN, HIGH); // RS high to avoid reset
programDAC8812(1, 0xFFFF); // Set channel A to midscale (32768, mid value of 2^16)
// programDAC8812(2, 0x4000);
}
void programDAC8812(byte channel, uint16_t value) {
uint32_t command = 0x00000; // Nota: el tamaño debe ser al menos 18 bits, por eso se usa un uint32_t
// Configure the command based on the selected channel
if (channel == 1) {
command = 0b11 << 16; // Set DAC A (A1:A0 = 01)
} else if (channel == 2) {
command = 0b10 << 16; // Set DAC B (A1:A0 = 10)
}
// Combine the channel bits with the value
command |= (value & 0xFFFF); // Set the 16-bit value
// Print the full 18-bit command in binary
Serial.print("Channel: ");
Serial.print(channel);
Serial.print(", Value: 0x");
Serial.print(value, HEX);
Serial.print(" -> Command: 0b");
for (int i = 17; i >= 0; i--) {
Serial.print((command >> i) & 1);
}
Serial.println();
// Begin SPI communication
SPI.beginTransaction(DAC8812_settings);
digitalWrite(CS_PIN, HIGH);
digitalWrite(CS_PIN, LOW);
// Split the 18-bit command into SPI transfers
uint16_t firstPart = (command >> 2) & 0xFFFF; // Extract the upper 16 bits
uint8_t secondPart = (command & 0x3) << 6; // Extract the lower 2 bits and shift them
// Print the parts being transferred
Serial.print("SPI.transfer16: 0x");
Serial.println(firstPart, HEX);
Serial.print("SPI.transfer: 0x");
Serial.println(secondPart, HEX);
// Send the data via SPI
//SPI.transfer16(firstPart);
uint8_t byte1 = (command >> 10) & 0xFF; // Primeros 8 bits (de B17 a B10)
uint8_t byte2 = (command >> 2) & 0xFF; // Siguientes 8 bits (de B9 a B2)
uint8_t byte3 = (command & 0x3) << 6; // Últimos 2 bits (de B1 a B0) desplazados a la izquierda
// Enviar cada parte
SPI.transfer(byte1);
SPI.transfer(byte2);
SPI.transfer(byte3);
digitalWrite(CS_PIN, HIGH); // End SPI communication
digitalWrite(LDAC_PIN, LOW);
// Short delay for LDAC pulse
digitalWrite(LDAC_PIN, HIGH);
//digitalWrite(CS_PIN, LOW);
SPI.endTransaction();
}I hope you can help me.
Regards, Omar