Part Number: ADS1299
Tool/software:
I need to clear up a few questions:
1) How can I link BIASREF pin ADS1299 IC when I'm utilizing both unipolar and bipolar supply in my design? In both supply cases, is it possible to connect ground externally or can we set BIASREF_INT = 1 to obtain the average of ((AVSS+AVDD)/2) internally?
2)I'm measuring EEG and EMG using two ADS1299.ADS1299 will measure the EEG first, followed by the EMG. Both ICs have the ability to switch between bipolar and unipolar supply. Positive 8 channels of the EEG's single-ended input feed with inputs, while the negative channels are internally shorted to SRB1, which serves as our reference electrode. We are regarded as differential inputs for EMG, with the positive channel serving as the input and the negative channel as the reference. However, I'm not sure that
a) Is it possible to short two IC bias electrodes as one? How can I short if so? Should I supply two separate bias electrodes if not?