Part Number: ADS7953
Tool/software:
Dear Sir
we are facing the following problem: MXO pin is never equal to the selected Ch.
Given that in idle condition we see MXO at 3.3V
When i want to read the ADC, for instance CH4 (forced externally to GND), the MXO moves from 3.3V to the expected CH value, but pin MXO do not show 0V, but an offset of about 0.5V.
See below: Yellow is the MXO pin and red is the SDI pin

See below the schematic
Notice that we have same result also bypassing the opamp between MXO and AINP (i.e.: mounting R118)
Notice also that if we separate MXO from AINP (AINP floating), however the issue is present on MXO, never equal to the selected channel...
We also tried other channels: CH1 is expected to be a steady 1.2V (measured with multimeter) Instead MXO reports almost 3.3V
Any clue on what's happening?
Andrea