This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDC264: DDC264 Read data via SPI

Part Number: DDC264


Tool/software:

Hello, I am trying to receive data from DDC264 to STM32 MCU

I established protocol according to the manual in the attached picture you can see the image from the oscilloscope 

But I didn't receive any meaningful data it is just a random values. 

Reset pin from DDC264 connected to 3.3V

For "CLK" from DDC264  established frequency -   2MHz 

I didn't write any registers to DDC264 I just want to read data from DDC264 with factory settings. 

So how work now 

  1. Detect when "DVALID" moves from 1 to 0 
  2.  Start reading 128 bytes via SPI 
  3. Toggle "CONV"

    the script looks like that 
    HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1);  // for CLK
    
    
      while (1)
      {
    	 
       	 	 if (HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_6) == GPIO_PIN_RESET)  // detect 
       	 	            {
    
       	 		        HAL_SPI_TransmitReceive(&hspi2,(uint8_t*)&test_64,&received_Byte_64,128,0x100);
    
       	 		        data_bytes[1] =	received_Byte_64[127];
       	 		        data_bytes[0] =	received_Byte_64[126];
       	 		        dataPacket = (data_bytes[0] << 8) | data_bytes[1];
      	 		        send_data_by_uart(dataPacket);  // only send firts channel 
    
       	 		        HAL_GPIO_TogglePin(GPIOK, GPIO_PIN_1);  // Toggle CONV  
       	 	            }
    
         }

Can you tell me where the error might be?

Regards, Ildar