Part Number: ADS1232REF
Tool/software:
Hello, I'm working on ADS1232REF and writing this topic for confiming a situtation. I read different voltage values with unexpected ratios. such as with gain 64 and calibrated 20 mV to 20 grams and gave different voltages from terminal, here are the values I get
| 20 mV | 25 mV | 30 mV | 35 mV |
| 19,97 grams | 23,97 grams | 26,97 grams | 29,75 grams |
As you see there is a no ratio between this numbers. Also I tried with a loadcell (4 pins, differencial), and get unexpected values about mass calculation. I believe there might be a problem about my board. if I'm mistaken, can you explain why. the other issue is I gave 20 mV with differencial but read 10.05 mV in screen and desktop applicaiton. I'm sure that there is no problem in my signal generator because I measured the given voltage values with different osiloscope.
Thank you for your answers.