This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS114S08: Random ADC values when one of the RTD is not connected in Two channel of 3-wire RTD Sensor with the ADS114S08B System

Part Number: ADS114S08

Tool/software:

Hello everyone,

I am currently working on designing a circuit using the ADS114S08 for measuring temperature with four 3-wire RTD configurations.

Our system consists of one SAMD21E17A MCU and two ADS114S08B ADCs. Each ADS114S08B is used to measure two 3-wire RTDs. When one ADS114S08B has only one RTD sensor connected to the corresponding input channel while the other input channel remains unconnected and floating, the ADC readings of the unconnected channel are unpredictable and fluctuate. This issue has been cross-tested with the same results.

Thank you in advance for your professional advice. I look forward to your insights.

RTD1:unconnected

RTD2:unconnected

RTD3:unconnected

RTD4:connected (16bit value = 7150, about 23℃)