Part Number: ADS7861
Other Parts Discussed in Thread: TLV9152
Tool/software:
Good Day!
What is the correct capacitance to ad on REFout pin for the ADS7861?
In the datasheet (SBAS110D) page 8: "(the internal reference can typically source 2mA of current load—capacitance should not exceed 100pF)"
But in the EMC User's Guide (SLAU094A) on page 7 in the schematic a 470nF is connected to the REFout pin.
That's why I'm asking this question. Also, we are using the ADS7861 in an older design (in single-ended configuration -> REFout, REFin and the negative channels are connected) with a 100nF, which works fine.
Kind regards