Tool/software:
Hello everyone,
I'm struggling to understand the input setup of the ADS125H02 ADC. I want it to be usable for single-ended and differential measurements. Differential measurements should be done through AIN0 and AIN1 and single-ended between AINCOM and AIN0/1. Is a setup like this feasible/recommended or not? Specifically, I'm wondering about the components before the input. The PCB Layout Example (fig. 103) places a 10 nF cap between AIN0 and AIN1. What is the purpose of this capacitor? I would assume than when changing to single-ended measurements, this cap will cause coupling of both signals. And should AINCOM be tied to ground in this case or does it make sense to have it floating for any measurements (symmetrical supply, so that GND is in the middle would allow for positive and negative voltages)?
Furthermore, I have some questions unrelated to the title: The example design (ADS125H02EVM) places 47 Ohm resistors in the CS, start and reset signals whereas they are not included in the PCB Layout Example (fig. 103). Are these needed or are they implemented "just in case"? Additionally, fig 103 recommends to tie CLKIN to GND behind a 47 Ohm resistor to use the internal oscillator. Can't the connection to GND be made without the resistor?
Thank you very much!