Part Number: ADS114S08
Tool/software:
Hii Team,
We are using the ADS114S08 for RTD temperature measurement and encountering an issue. The device works correctly and provides accurate temperature readings when all four channels are connected simultaneously. However, when any channel is disconnected, the next channel shows inaccurate values.
For example, when the RTD on channel 3 is removed, the values on channel 4 become distorted (off by 2 to 3 degrees). Similarly, when the RTD on channel 2 is disconnected, the values on channel 3 are affected.
Additionally, when we attempt to read the ADC in reverse order (channel 4-3-2-1), the value of the previous channel gets affected.
Could you please help us identify the cause of this issue and suggest a possible solution?
Attaching schematics for reference. (Pull together resistor of 1Mohm is DNP)
SCHEMATIC_SCU MICROCONTROLLER CARD REV B(2MM).pdf
Thanks
Nikhil Batra