Other Parts Discussed in Thread: ADS1231
I designed and manufactured a weight module with ADS1231 IC and it's not working. I think I put a wrong capacitor (C7, part number: 04023C104KAT2A) in-between CAP pins. Also the capacitors between AINP1 and AINN1(C4) and VREFP and VREFN (C9) are wrong. I copied a circuit that works and these are the values it has, but in my design it doesn't work. Is there anything I can do to make this work? replace the caps? C7 is 0402, the cap i need is in 1210 package...