This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE58JD48EVM: Query regarding the Equalization capabilites of AFE58JDEVM

Part Number: AFE58JD48EVM
Other Parts Discussed in Thread: AFE58JD48,

Tool/software:

Hi, 

We are working with AFE58JD48EVM, we want to test 160X mode at 78.125MSPS samling rate, which corresponds to 12.5Gbps lane rate. We are oprating at 312.5 MHz device clock on the FPGA side and ADC sampling clock as 78.125MHz. But we are getting 8b/10b disparity errors and not in the table error on the receiver side. So we want to explore the TX equalization capabilities of ADC but the datasheet doen't mention about the equalization supported on the TX side, also the EVM GUI doesn't have any option. So we wanted to confirm whether AFE58JD48 supports equalization on the serdes lanes ?