Other Parts Discussed in Thread: LMK04828,
Tool/software:
We are using ADS54J60 ADC IC and LMK04828 IC. The register configured are mentioned in the attached file. The rx_samples_valid signal is not going high. I am using 4244 ADC Mode with no decimation. I have observed that the pull-up voltage in INAP, INAM, INBP, and INBM are 2.8V initially and after hardware reset its 2.6V is there any problem in such case.
The schematic and the changes in the IP core is given in the attached file. Please let me know if any changes are needed.ADC_Query.docx
Thank You,