Other Parts Discussed in Thread: TSW14J58EVM, ADC12QJ1600
Tool/software:
Dear TI team,
I am using a TSW14J58EVM and TSW14J58 boards to implement the JESD204C protocol with the TI JESD240 IP. I used the ADC12QJxx00 GUI (Version 1.2 from 30 March 2021) to program the ADC (ON board oscillator, Fs=1000 Msps, JMODE8) but the TRIGOUT Clock Output is not stable (varies from 70-79 MHz and not 386.71875MHz that I was expecting for RX_DIV=32) and FPGA MGT QPLL never locks. Checking the ADC pll on the GUI is not locked either (V=3, P=4, N=20) and the RX_DIV is fixed at 64.
Because of this issue: https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1354764/tsw14j58evm-tsw12qj1600evm-interfacing-with-tsw14j58evm-having-a-issue-with-capturing-the-data
I tried also the python script. I modified it to get the SN and the output looks like this:
***************************************************************************
Initializing ADC12QJ1600 instance with defined attributes
Got Init Bit
ADC device initialization complete successfuly
ADC is ready for programming
***************************************************************************
***************************************************************************
Initializing ADC12QJ1600 instance with defined attributes
Got Init Bit
ADC device initialization complete successfuly
ADC is ready for programming
***************************************************************************
P = 2, V = 4, N = 20, FVCO = 8000000000.0
Setting the ADC's JMODE to 8
P = 2, V = 4, N = 20, FVCO = 8000000000.0
Setting the ADC's JMODE to 8
Done
But I don't see any change to the TRIGOUT Clock Output frequency. I don't even know if the script works since I tried to do some single register reads and always returns 255.
I noticed also that on the carrier board the PLLREFO clock is not routed at all. In this case I have to use the on-board oscillator to generate the free_running (125 MHz) and system clocks (12.375/33= 375 MHz for line rate of 12.375 Gbps, 64b/66b and line rate of 32 bits) according to the 6.4.7 of the TI204C-IP JESD FPGA IP User Guide.
Could you please help me with this?
Thank you in advance,
Panos