Other Parts Discussed in Thread: TSW1418EVM, ADC3683
Tool/software:
Hello TI Support Team,
I am currently using the TSW1418EVM to evaluate the ADC3583 with a 2-wire SLVDS interface. The setup is being tested using the High-Speed Data Converter Pro (HSDC Pro) software to visualize the output waveform.
However, I have observed what appears to be ripple noise or unintended fluctuations superimposed on the waveform in the output data. This noise makes it difficult to interpret the signal accurately.
I would greatly appreciate your advice on potential causes of this ripple and suggestions to mitigate or eliminate it. Could this be related to power integrity, signal integrity (e.g., SLVDS termination or routing), or some other configuration issue in HSDC Pro?
For your reference, I have attached the schematic, data capture setup, and configuration files related to the test.
Thank you for your support and guidance.
,
Number of Channels | 2 | ||
Number of Bits | 16 | ||
ADC Output Data Rate | 40MHz | ||
Particulars | Channel1 | Channel2 | |
Min | 32481 | 32768 | Codes |
Max | 54353 | 32768 | Codes |
ST Dev | 6809.53 | 0 | Codes |
Mean | 39469.22 | 32768 | Codes |
RMS | 9553.81 | 0 | Codes |
Peak to Peak | 21873 | 1 | Codes |
PAR | 1.17 | NaN | dB |