This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1232: Reading onboard Temperature Sensor

Part Number: ADS1232

Tool/software:

The issue seems to persist. The ADC generates a value of  415922, corresponding to a Voltage of 123mV (ADCout/ADC_MAX)*(Vref/2)

This would mean the chiptemp is at 25°C + ((123mV-111.7mV)/379uV/°C) = 56°C which is unreasonable directly after startup imo.

Could someone check where I went wrong? Or are the factors provided in the datasheet wrong?

Best regards

Damian