This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS131B04-Q1: RESET bit of STATUS reg is '1' every reading while reset pin is pegged to DVDD and null command issued

Part Number: ADS131B04-Q1

Tool/software:

does it normal behavior of the bit of the STATUS?

  • Hi Mykhaylo,

    You should be able to get 0x050F STATUS word when you reading the conversion from ADS131B04-Q1, "F" in this data indicates that the conversion data on all 4 channels are available and ready to be read. See the first word in the timing below:

    I would suggest you to check if there is any glitch to the START/RESET pin. If you could share a data file of your timing captured with a logic analyzer(for example Saleae), I can check it as well.

    BR,

    Dale