This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3669EVM: ADC3669EVM + TSWDC155EVM S/W F/W support

Part Number: ADC3669EVM
Other Parts Discussed in Thread: ADC3669, , TSWDC155EVM

Tool/software:

Hello,

I'm considering to purchase both boards for my project evaluation.

If I recall correctly, TI can send me the complete S/W and F/W for the boards once I purchase them.

Is the software HSDC compatible one? or Do you provide the Vivado demo?

I need to evaluate the Spectrum domain up to 250MHz range and sine waveform construction from the ADC3669 channels.

Please give me details of the S/W and F/W so that I can happily purchase the boards.

Kind regards

DK

  • Hi DK,

    We will provide you with a software package with an example python script that will setup the ADC and FPGA, and capture data in HSDC Pro.

    You will need to purchase an ADC3669EVM and a TSWDC155EVM capture board, as you have mentioned. I am going to go ahead and close this post, and I will reach out via email and provide you a link to download the software package.

    Best,

    Luke Allen

  • Thank you for providing all the  APIs and manual! Last week we've purchased the boards. Looking forward to grab the boards!