Tool/software:
Dear Sir
We are having synchronising issues on the AFE data.
We suspect it is the AFE not resetting correctly.
We follow the device initialization as per the documentation:
Device Initialization
After bringing up all the supplies and applying a RESET signal, follow these steps to initialize the device:
1. Write all bits marked 1 in all the register maps (which is only 5 bits: reg 3, D1, D4)
2. The following steps initialize the PLL:
1. 100 μs or later after the clock starts and after applying RESET, write the PLLRST1 and PLLRST2 bits to 1
2. Wait for at least 10 μs and then write the PLLRST1 and PLLRST2 bits to 0
Above PLL initialization must be done whenever the device comes out of a global power-down mode or
when ADC_CLK is switched off and turns on again.
3. Apply a TX_TRIG pulse to synchronize operation across multiple devices.
However in 1% of reset cases, the data from the various channels may be unsynchronised.
This occurs even at very low speeds (with a 10MHz AFE clock)
As per the SWAROOP board, with 2 AFE, and 4 TX, if we display the data as a B-Scan, we can see the error as per the attached image.
Here we have channels 1 to 128.
Channels 1 to 32 and 64 to 96 are the same AFE channels due to symmetry.
Has this issue been identified by anyone else?