Tool/software:
Hi
We are looking the part SN74LXC2T45 for signal level translation. Propagation delay is our key parameter for design.
There is given Minimum propagation delay (with VCCA= 3.3 ± 0.3 V) as 1ns and Max propagation delay as 57ns (From A to B) with -40°C to 85°C and 36ns with -40°C to 125°C and min 1ns and max 33ns and 29ns respectively with temp. It is also decreasing (Max value) with VCCB increasing.
What is the key factor responsible for this propagation delay. What propagation delay we should consider here. Can you please help here to understand this.
Can we change VCCB/VCCA supply in steps of 100mV with VCCA/VCCB (3.3 ± 0.3 V) fixed voltage respectively. We need to translate 3.3V signal level to 1.1V to 5V with 100mV steps (like 1.1V, 1.2V, 1.3V.......4.9V, 5V).
Best regards