Part Number: ADS124S08EVM
Other Parts Discussed in Thread: ADS1220EVM, ADS124S08
Tool/software:
Dear Specialists,
My customer is testing ADS124S08EVM and has questions.
I would be grateful if you could advise.
---
I have obtained the ADS124S08EVM and am evaluating, I have some questions.
Could you please advise?
I would also like to ask the same thing with the ADS1220EVM.
If your answer is different from the ADS124S08, please comment.
1. When using the Delta-Sigma ADC Evaluation Software to connect a 3-wire Pt100 to measure temperature, how do I convert the code value and voltage value displayed in the Data Analysis tab to temperature [℃]?
2. I am measuring by selecting 3-wire RTD in the Scripts tab, how do I change or check the conversion time?
(My coworker previously asked about the conversion time in this email, and I would like to check it with this evaluation board.)
3. When selecting 3-wire RTD for measurement, how do I change the filter selection?
4. I understand when switching between the 2 channels of the ADS124S08, it was stated that the settings must be switched for each channel
Is it possible to check the conversion time by making similar settings on the evaluation board?
Also, is it possible to do this with the ADS1220EVM?
5. What does 2048 points/samples mean under Collect Data in the bottom right of the Data Analysis tab?
What will change if I change this?
6. Are the code and voltage values displayed on the Data Analysis tab raw values?
Are they averaged internally and then output?
---
I appreciate your great help in advance.
Best regards,
Shinichi