Part Number: ADS7957-Q1
Tool/software:
Each channel (ch0~ch15) receives and processes 0~5V input according to the temperature sensor status.
The voltage input to each channel does not fluctuate, but the temperature value displayed in some products fluctuates severely, so we are checking. We recognized it as cold soldering and replaced and reworked the parts (SMT), but the same symptom is occurring. (There is no abnormality in the voltage input to the circuit.)
Do I need to connect GPIO2 related to the RANGE setting? The circuit is currently not connected (floating).