Tool/software:
Subject: UCC28600 – Observed Burst Switching Behavior Not Matching Datasheet
Question:
Hello,
I am using the UCC28600 in my power supply design and I have observed a switching behavior that I would like clarification on:
-
In my measurements, the burst switching frequency is ~130 kHz, and the burst-to-burst frequency is ~1 kHz.
-
During this operation, the feedback (VFB) voltage cycles between 0 V and ~1.7 V.
As per the datasheet:
-
In burst mode, the expected burst frequency is around 40 kHz, and
-
The feedback voltage should typically be below 0.7 V.
Because of this, my observed operation does not seem to fit into either burst mode or frequency foldback mode (FFM) as defined in the datasheet.
My question: Which operating mode of UCC28600 corresponds to this behavior?
Any guidance or explanation from TI experts would be very helpful also sugest posiible recomendation to resolve this problem.
Thanks,
Ashish