3857.Video Input Block Diagram.pdf
Hello,
I am interested in recommendations for an NTSC/PAL video decoder. Please see attached for block diagram. The application is taking up to four (4) NTSC/PAL video inputs, decoding to one of many possible digital output formats, and going to two camera interface ports on the i.MX53 Freescale processor. The goal is to be able to display any two (2) of the four (4) video inputs at any one time on our LCD display.
This decoding device can come in one of two forms:
1) 2:1 MUX at Qty 2 per assembly
2) Dual 2:1 MUX at Qty 1 per assembly
Optional item is to have internal hardware de-interlacing available in the device; however, this is not a hard requirement. Please let me know if you need any additional information.
Any feedback or input is welcomed and appreciated!
Thanks and best regards,
Paul