Part Number: ADS7924
Hello,
We are using ADS7924 for data conversion. We have Voltage(0V-3.3V) and Current inputs(4mA - 20mA) given to different channels of ADS7924. I want to use Manual Scan mode in my application but I am facing issue with Manual Scan Mode. I need help regarding the same.
The ADC Channels are configured as Ch1 - Voltage1, Ch2 - Current1, Ch3- Voltage2, Ch4- Current2.
During testing we have given current input to ADC Ch4, remaining channels left open. And We have set mode to Manual Scan Mode and Channel Selection is set to 4 i.e. We have written 0xCB to 00h register. During this configuration we are getting less fluctuations in ADC output. But if I write 0xC8 to 00h register(Manual Scan mode with Channel Selection set to 0), we are getting more fluctuations in ADC output. Why is the channel selection causing issue in our ADC readings.
We have set 50 Micro Seconds as ACQTIME. And we have a 500miliseconds timer configured to read all channel ADC data continously. After reading all the channels data, we are trigger manual scan at the end. So again after 500ms only we will initiate the read and so on.
Please suggest us which channel will be more efficeint for our application.
Thank You.
Regards,
Balaji