Part Number: DAC61416
Hi exparts,
The following is described in the CRC error check section of the DAC61416 data sheet.
"After the write command, a second access cycle can be issued to determine the error checking results (CRC-error bit) on the SDO pin."
- This means that the error check frame including CRC-error will be returned from the SDO pin when cs is lowered after the Write command?
- Is there a way to use SDO only on a the Read command?
The background to the above question is as follows.
- CRC check required to ensure data integrity -> Monitor with ALMOUT instead of SDO readback.
- Want to monitor Read command Ack to see the health of the DAC itself -> Enable SDO-EN for Read command.
- When SDO-EN is enabled, read back occurs during the Write command, and write cycles take twice as long as expected.
If there is a way to solve the problem of increasing the write cycle other than the above 2, please let me know.
Regards,
Hiromu