ADS8598H: driver code for ADS8598H to interface with TMS570LC4357

Part Number: ADS8598H
Other Parts Discussed in Thread: TMS570LC4357,

Hi Team,

We are using the external ADC ADS8598H and would like to request the source code to interface it with the TMS570LC4357.

Additionally, we need details on the register configuration to enhance communication, along with the SPI command sequence for transmitting and receiving data.

 

Thanks

Kusuma

  • Hi Kusuma,

    Thanks for your question. We do not have any reference source code for this device. The datasheet should have the information you are looking for about SPI sequence for read and write (section 7.4.2.3). The ADS8598H does not need register writes, but rather the features are controlled by the pins described in section 7.4.1 of the datasheet.

    Best regards,
    Samiha