Part Number: ADS131M08
Other Parts Discussed in Thread: ADS131E08
Hi Experts,
I'm Using the ADS131M08IRSNR and I've used an external voltage reference of 3V.
After sampling my device with the ADC I've wanted to use the external voltage reference so I've disconnected the 3V and changed it to an internal voltage reference.
When I'm testing the voltage on the REFin line im getting 1.176V [instead of 1.2V +/-0.1%] and the reading that I'm getting from the ADC are wrong.
The reason that the internal reference voltage I'm measuring is wrong is because I've set high voltage reference? because in the datasheet it says that you can set the REFIN as high as VDDA+0.3V which in my case is 3.3V.
The 2nd thing is why am i getting the readings so wrong? for GAINx1 the calculations should be (VALUE*1.2V)/2^23, am i getting it wrong? The OSR is at max value [16,384], The exrenal clock set for 8.182MHz.
Another question about filtering the signals when I'm designing my board -
I saw when you want to use anti-aliasing you should connect the differential inputs like that -
Those values are stay the same for any current I want to measure? because in my case I want to measure small currents from 1uA to 200uA [R_L is 1kOhm] and i would like to know what is the best application in my case that the currents are measuring will be as quiet as they can be with this ADC.
Regards,
Bar