This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE20408EVM: DAC output is not changed

Part Number: AFE20408EVM
Other Parts Discussed in Thread: AFE20408

Hi,

My customer is evaluating AFE20408 on the EVM with GUI.

When the customer change the DAC value on GUI, the DAC output is not changed at DACA0 to 3..
Could you give us any advise to solve it?

The attached pdf shows the GUI settings.  Please refer it.
At the setting, DAC output voltage was -5V at DACA0 to 3.  The customer changed the buffer value on the GUI, but DAC output voltage is not changed.
VSSA = -5V and VCCA = 0V.
The customer refered user's guide to set the GUI.  If you also give us any other documentation of usage of the GUI, it helps us.

ScreenShot.pdf 

Best Regards, Taki