From the datasheet(DAC5670-SP),there are some porblems i can not utterly understand.
1.when i use the FPGA as a data source, whether the DTCLK_P/N of the DAC5670 as the sampling clock when the DAC5670 receive the datas from the data source or not. 2.In the page 15,how much the value of the resister i should select at the terminal of IOUT_P/N .
3.In the page 15,which the mode of 1:1 balun i should select at the terminal of IOUT_P/N . Is the TC1-1- 13MA+ ok?
4.In the page 15,which the mode of balun i should select between the single-ended clock and differential clock(DACCLK_P/N),and can you recommend a chip used to generate the single-ended clock?
5.Are there evaluation board schematics about the chip of DAC5670-SP?