This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP2234 and ADS1115 - How to design an ADC driver?

Other Parts Discussed in Thread: ADS1115, LMP2234

Hello folks,

I'm working in a design with low (uV) analog signals that must be converted to digital. I have already designed the AFE which raise the signal to 100mV - 1V orders of magnitude. After the AFE stage, the circuit has a unity-gain, low-pass filter that serves as an anti-aliasing filter. The AFE + LPF are implemented using a LMP2234 op amp. Then, the signal is fed to the ADC (in this case I'm using ADS1115, 16-bit Sigma-Delta ADC).

My question is if this topology still needs to have a ADC driver, or does the LPF servers as the ADC driver?

Thanks in advance,

André Araujo.