This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
From the datasheet DAC5670, I found that the chip have 2 pins of“IOUT_P” (A7,B7),and have 2 pins of “IOUT_N” (A10,B10). What should i deal with the 4 pins ?
Are these 4 pins used as a pair of differential outputs, or two pairs of differential output ? If i connected the 4 pins in accordance with the following diagram ,is it right ?
These pins have double pins to reduce inductance. Your connections are correct.
Regards,
Wade