This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm using a ADS1281-EVM for a high-precision weighing scale, using electromagnetic force compensation.
The samples from the ADS1281 with 250S/s are downsampled to 1S/s. Therefore our interesting frequency band is from about 0.01Hz to 0.5Hz.
In this range the input amplifier (with the external componentes) used in the eval-module has a noise voltage of about 100nV! This is much more than I will expect from the analog circuit, which should be measured with the ADC.
For the analog circuit of the scale I'm using the Zero-Drift OP from Analog Devices (ADA4528-1), which has no 1/f-noise.
Do you have any suggestions for a replacement of the OPA1632, which has no 1/f-noise? In best case is will also have the same footprint, so i can replace it on the EVM.
kind regards,
Karl Zeilhofer
Hello Karl,
Welcome to the TI E2E forums!
Any chopping or auto-zero amplifer will have practically zero 1/f noise. See the OPA188 or dual version OPA2188.
The downside of using the OPA188 or ADA4528-1 is that they are not of the differential output type, like the OPA1632. However, you could build a fully differential amplifier using the dual OPA2188.
Note: The OPA188, OPA2188, and OPA1632 have the similar packages but different pinouts.
Regards,
Chris