Other Parts Discussed in Thread: ADS8568, ADS8556
Dear All,
I started to design precision DAQ system based on ADS8568SPM. I also used REF5025IDGK as a precise voltage reference. I have two ADCs. in same PCBs and a microcontroller manages ADCs and collects digital data. ADCs are used in daisy chain mode and SDO_A is only output for 16 channels. All channels are used simultaneously. Same Convst, SCLK, SDI and Frame sync. signal will be applied to both ADCs.
I have some questions as follows.
1- ADCs are used in daisy-chain mode and first ADC DCEN pin (# 23) is tied DGND second ADC DCEN pin is tied DVDD. The datasheet says if DCEN = 0, DCIN_X pins should be connected DGND. However there is not any explanation when DCEN = 1 and DCIN_B,C and D are not used. Second ADC DCIN_A input is tied first ADC SDO_A output. Other inputs won’t be used. I think DCIN_B,C and D should be connected to DGND. Am I wright?
2- AGND and DGND are separated in my design. I will make ground plane for both GND. Normally I will connect AGND and DGND only one point where as near as possible to power supply. Power supply will be on another PCB or backplane, but I try to make quiet ground for AGND. On the datasheet Page 44 the recommended layout is not clear for me. I think thermal pad (heatsink pad) is connected to AGND and also DGND over vias. That means AGND and DGND connected each other where near ADC. What is the best practice for connecting AGND and DGND?
3- I attached the schematics in pdf format. The ADC and Vref part are nearly same in Evaluation Board. I made small changes. Please check it if there is any inconvenience.
Best Regards,