This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am new with working with DAQ systems, I am currently working with the LIS344ALH accelerometer which has a resolution of 50 (ug/Hz-1/2) and a dynamic range of +-2g with enough bandwidth of 50 Hz. The ADC is 16 bit so it is close to the accelerometer resolution.
I would like to know how can I try the ADS8341 with the LIS344ALH in a evaluation board that has a LP filter and gain amplifiers. And if it is possible, a cheap one.
Thanks a lot,
David.
Hi Abhijeet,
Thanks for the quick reply.
I need a 16 or more bits ADC for my accelerometer app. I am using a LIS344ALH analog accelerometer that has noise density of 50 ugHz-1/2, so I need quite good resolution from the ADC too. Also, I need to filter the signal at 50 Hz before amplifying it so it gets to the ADC without noise input above 50 Hz. The evaluation boards are quite pricey for me, is there any know design I can follow to use the accelerometer with the ADC and connect it to the MSP430 MCU that I am also buying?
Is there any quick way of designing that kind of DAQ circuit?
Please, I am new to DAQ circuits design , all the help will be highly appreciated.
Thanks,
David.
Hi David
Sorry for the delay in the reply !
The best possible option I can think of is to have an external filter followed by 16 bit device similar to ADS8684. The quickest possible way to design this to have an EVM and interface with your sensor board or create your own proto board with ADC.
Thanks & Regards
Abhijeet