Other Parts Discussed in Thread: DAC7742
Hello,
I have a question about DAC7742.
There is a possibility that is occurring the latch-up at DAC7742.
Because, The REFout is reduced to 30% of the original output.
As a result, The Vout reduced to 30% from original output voltage.
Vout & REFout is usually 10V output.
a, Power up sequence of error condition
Vdd -------> Vcc -----> Vss
(20ms) (1ms)
b, Power up sequence of nomal condition
Vdd -------> Vcc -----> Vss
(1s) (2-3ms)
(Question)
1, Please tell me why the output voltage of Vout and REFout becomes abnormal.
2, In the error condition,Output voltage of Vout and REFout has been reduced to about 30%.
Is there a reason why the output voltage becomes 30%?
Best Regards,