Other Parts Discussed in Thread: ADS5263, THS4131, ADS5263EVM, ADS5295
Hi,
I use the ADS5263 in single ended mode for the sample CLK.
CLKM is tied to ground and CLKP is tied to a signal 0 to 3.3V of frequency 12.5MHZ (50% duty cycle).
The reset phase off the ADS5263 seems to be ok and I can also write or read the configuration with the serial interface.
So, the problem is the frequency at the output LCLKP, LCLKM is about 5KHz (without a stable duty cycle) and the the ADCCLKM and ADCCLKP is also affected by the same problem (with a lower frequecy).
Do you have any information or suggestion of what could happen?