This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The 7809 is characterized for operations from 4.75V to 5.25V. The resulting power supply sensitivity (over temperature) is 8LSB (or 16LSB/V).
If the supply votage exceeds 5.25V (e.g. to a maximum of 5.35V), what is the effect? I.e are there effects other than just a proportional increase in error?
The inference I make is that it could add approximately (5.35V-5.25V)*16LSB/V=1.6LSB of error. Is this a valid inference?
Hi Richard,
From talking to our designer, most of the PSS is due to headroom limitations that become important when the supply voltage falls below the nominal 5V. In other words, the ADC output would probably show a larger offset when the supply goes below 5V than when it goes above. For this reason, we expect the ADC's sensitivity to a +0.35V vs. a +0.25V change in its supply voltage to be minimal. Although we cannot guarantee an upper limit, we think that your "linear" estimate may be conservative. I hope this helps.
Best Regards,
Harsha