Other Parts Discussed in Thread: DAC8581, TINA-TI
Hello,
I would like to know if there is any DAC8581 SPICE, VHDL or verilog model available ?
I would be able to run a mixed-signal simulation in order to validate my DAC8581+filter measurements.
I am using my DAC8581 under the following conditions :
* Power supply : +/-5V
* Voltage reference : 3.3V
* Sample rate : 2MSPS
* Signal is around 20% of Full-scale
In order to filter DAC8581 output at 200kHz, I use a 3rd order passive filter in the following configuration :
(DAC8581 is driving Vout1 node ; output is observed on J1 SMB connector)
I observe a very high THD(~-20dB) at the filter output.
Then I would like to be able to simulate DAC8581+filter assembly transient response in order to validate my filter.
Thank you for the support
Gwenael.