This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ads1131 schematic evaluation

Other Parts Discussed in Thread: ADS1131

Hi,

Attached is a schematic of ADS1131 in a ratiometric design.

Can you please check the VREFN pin and comments of overall design if any ?

Regards,

Theodore

Schematic Prints.pdf

  • Hi Theodore,

    You have a 60cm cable and no true input filtering. You really need to consider the effects of gaining up external noise relative to the noise of add resistors that is picked up on the cabling.  This is true for both the reference and analog inputs.

    Differential caps are more important than the common mode caps. 

    The PSW will connect the excitation path to ground, so C21 is really not necessary when VREFN is at ground.

    Best regards,

    Bob B