This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Questions about ADC128S052Q

Hi,I'm disty in Japan.

My customer is considering using ADC128S052Q to next model.

I have three questions about ADC128S052Q.


①Which voltage is used for a reference voltage for the charge redistribution DAC, VA or VA/2?

②Is the reference voltage for the charge redistribution DAC held during AD conversion,
   or is it input in direct to DAC?
    (I would like to understand that whether the reference voltage for DAC fluctuates
     when the VA voltage fluctuates during AD conversion. )

③If a voltage of approximately 2V(the input current is limited to below 2mA) is applied to
   analog input pin(IN0 to IN7) under the conditions of the VA/VD=0V,will this device be damaged? 
     


Best regards.

  • Tokumoto-san,

    This thread has been moved to the Precision Data Converters forum for more appropriate support.

    Regards,
    Eric Hackett
  • Hello Tsuyoshi,

    #1. I believe VA, since it needs to be able to swing above and below VA/2 to balance the charge on the sampling cap above and below VA/2.

    #2. No. The ADC128S series is a SAR (Successive Approximation) converter, which compares VA/2 and VC as "Higher" or "Lower" for each clock cycle until it reaches the LSB.

    The reference voltage is NOT regulated or sampled internally. Any changes in VA will affect the VA/2 reference into the comparator, and thus the current reading during the last 13 clock periods. This is why it is critical that the VA be clean, stable and well bypassed to achieve optimum performance.

    #3 There are ESD diodes from the inputs to VA. See Figure 37 on page 16. If VA is below the input voltage, the upper ESD diode will forward-bias and clamp to the VA. The ESD diode is taking the current and must be limited to less than the Abs Max input current (10mA). I would limit to less than 1mA - or about 1K series resistance for every volt over VA.

    Note that if there is enough current available at the input, this may cause the VA line to be pulled up to a random voltage (until something on the line starts to conduct). If this is condition is expected to occur regularly, a clamping Zener should be used on the VA line to ground (to prevent the VA line from being pulled too high), and a Schottky diode between the input and the VA line to take the stress off the internal ESD diode.

    Regards,
  • Hello Paul,

    I appreciate your prompt reply and detailed explanations.

    I understand your answers.

    Please let me ask you additional two questions.


    I tried converting an analog signal to a digital value with method of SAR
    by manual to confirm the effect of the VA fluctuating during AD conversion.
    *Cf. attached file adc_result.xlsx

    adc_result.xlsx

    Question 1)  Is method of my conversion correct?


    From the file of "adc_result.xlsx", when I compared the ADC result of the case of the VA
    fluctuating during Hold/Conversion mode and the case of the VA fixing,
    the both results were same(0x804h).

    My thinking is as follows.

        When the VA which is the reference voltage of DAC fluctuates during Hold/Conversion mode,
        the comparison voltage VA/2 also fluctuates in the same way.

        As a result,an error by the VA fluctuating during Hold/Conversion mode decreases relatively.

        However,the VA fluctuating during Sample mode affects the ADC conversion result.

        As my conclusion, the VA fluctuating during Hold/Conversion mode does not have a big effect
        on the conversion result, but the VA fluctuating during Sample mode affects the conversion result.

     Question 2)  Is my thinking correct?

    Please lend me your expertise!


    Best regards.

    Tsuyoshi Tokumoto